Southwire’s SWRate is a widely used software tool for calculating steady-state and transient line ratings for overhead conductors. The program ships with orders of Southwire’s Overhead Conductor Manual. Used jointly with Southwire SAG10®, SWRate allows for complete modeling of an overhead conductor.
The newest version of SWRate, version 4.1, includes these upgrades:
Southwire continues to keep its software up-to-date based on current knowledge of line rating calculation methods and evolving industry standards.
Specifically, Southwire is committed to keeping SWRate compliant with IEEE Standard 738, which covers calculation of current-temperature relationships in bare overhead conductors. SWRate versions 3.02 - 4.0 comply with the previous 2006 revision of Standard 738. When the proposed Standard 738-2011 is adopted, Southwire will be positioned to ensure that SWRate is compliant with it.
For more information on SWRate v4.1, contact Southwire here.