New industry standards focus on MV application categories. The changes present a rare opportunity for reviewing internal company standards.
Industry standards for medium-voltage power cable typically evolve slowly – and the opportunity to do a substantial review of a company’s purchase specifications comes rarely.
“Now that opportunity is available,” says Dave Mercier, technical director of Southwire’s Electrical Division. “ICEA (Insulated Cable Engineers Association) has replaced their key industry standards with a new set that is organized differently. The new organization will require changes in purchase specifications.”
The new ICEA standards for power cable have been reorganized to focus on cable voltage-range and application categories rather than insulation materials. The advantage of this approach is that all insulations suitable for use in a specific application can be contained in a single document. (See tables 1 and 2.) The new standards also reflect the latest wire and cable construction practices, insulations, and jacket materials.
Industrial wire and cable purchasers typically specify ICEA standards to augment the requirements of UL 1072, Safety Standard for Medium-Voltage Power Cables. This UL document is still the minimum requirement for power cables used under the NEC. The ICEA standards document additional requirements such as dc voltages for field tests, emergency overloads, and minimum bending radii for cables.
“In step with ICEA, UL has added updates to UL 1072,” Mercier says. “The third edition of UL 1072 incorporates and harmonizes with the majority of the changes in the ICEA standards.”
In addition to ICEA standards, specification writers can call out industry-standard qualification testing defined by the AEIC (Association of Edison Illuminating Companies). Qualification testing is contained in AEIC CS-8, a new specification that also harmonizes with the new ICEA standards. CS-8 replaces the earlier AEIC CS-5. “CS-8 was written for the utility industry, so if you do reference it for industrial applications, make sure your wording makes it clear that you are only referencing the qualification-testing portion,” Mercier advises.
“As specification writers update purchase specification to reflect the new industry standards, they should also take advantage of this opportunity to do a thorough review of their company’s internal standards, just as ICEA did,” says Mercier. “This is a rare chance to review and update the company’s position on the type and quality of cable being specified, so it reflects current industry practices and improved manufacturing capabilities.”
Table 1. New ICEA/NEMA Standards For Power Cables
Table 2. Withdrawn ICEA/NEMA Standards For Power Cables
Key Standards Groups For Wire And Cable
| ||||||||||||||||||||||||||||||