Superconductive Power Distribution Comes of Age: Two and a Half Years of Successful Commercial Operation

On February 6, 2009, Southwire Company and its partners marked the two-and-a-half year anniversary of an urban power distribution project using high-temperature superconductor-known as HTS Triax® Superconducting Cable systems.

The installation in Groveport, OH used approximately 200 meters (600 feet) of Southwire's HTS Triax Superconducting Cable to distribute electric power to 8,600 homes and businesses through American Electric Power's Bixby substation. In addition to American Electric Power (AEP), project partners included American Superconductor, the U.S. Department of Energy's Oak Ridge National Laboratory, and Praxair.

"Using second-generation cable design and recent advances in cooling technology, the Bixby installation proves the reliability of HTS Triax Superconducting Cable systems in reducing the cost of high-efficiency power distribution in an urban setting," says David Lindsay, Southwire Director of Engineering, Distribution Applications.

HTS Triax system works worry free

The system has experienced more than 75 transient events, including lightning strikes, during its 2.5 years of operation. Most of these events were through-faults -fault current that entered the Bixby station from the distribution circuits powered by the HTS Triax cable. No change in system temperature or pressure was recorded as a result of the events and the system has never been taken out of service as a result of these events.

The system has operated successfully since its installation in August 2006. Designed and built for a load rating of 3,000 Amps per phase, it performed at 90.5% of the design rating, reaching 2,715 Amps during peak loading in the summer months.

"Our partnership with Southwire has allowed us to test advances in superconductivity and cooling design on our system with virtually no interruption to customers," says Michael Heyeck, AEP Senior Vice President of Transmission.

The many benefits of HTS Triax Superconducting Cable

With the rapid decline in available underground space for conventional cables and the prohibitive cost of real estate for new or expanded substations, superconducting cables are emerging as a solution for electric power to densely populated areas. There are many benefits of HTS Triax superconducting cables, including: · Increased reliability in the electrical grid by facilitating interconnectivity between electrical substations and alleviates substation space constraints. These virtual substations can eliminate the need for some transformers saving a utility customer up to $2 Million per transformer. · HTS Triax cables add capacity to existing duct banks. One HTS Triax cable can carry as much current as 18 large copper cables. This is possible because HTS Triax cable operates at extremely low temperatures for power cable-281°F (-196°C)-and eliminates current flow resistance. · Large power transformers can be located further away from urban centers because HTS Triax cables carry very high currents at lower distribution voltages. Additionally, valuable real estate for development and green space is freed up. · Reduced critical cooling requirements, combined with newly commercialized cryogenic cooling technology, reduces cost and maintenance. HTS Triax is very compact, with three phase conductors placed concentrically around a common central core, cutting the quantity of wire in half. This smaller surface decreases cooling requirements.

More Superconducting Cable installations are at work to support demand

According to Heyeck, "The performance of the HTS Triax system has shown the potential for cost savings with excellent reliability in a variety of applications."

With the Bixby performance success, Southwire now draws on over a decade of in field superconducting experience. Together with projects under way in New Orleans and New York City, these installations prove the in field success of urban delivery of critical electric power through superconductivity and position Southwire as an experienced leader in this innovative offering.

For more information on HTS Triax superconducting cable systems or the Bixby substation project, visit http://www.supercables.com.

Imagery is available to the press by contacting Kayla Smith at kayla_smith@southwire.com

About Southwire:
A technology leader, Southwire® Company is a major wire and cable provider in North America, manufacturing copper and aluminum building wire and cable, metal-clad (MC) cable, metallic and non-metallic flexible conduit, cord products, utility cable products, industrial power cable, power generation cables, copper and aluminum rod and continuous casting technology. Through innovative research, Southwire has developed and patented Flatwire Ready® SureSeal® HTS Triax® Superconducting Cable, SIMpull THHN® cable, Romex® SIMpull® cable and, MCAP® and HCF MCAP® cables. Southwire has also developed other innovative products such as Riser MC cable, HS285, Vibration Resistant (VR2) and PowerGlide® Utility Cables. Visit our website at www.southwire.com.

Press Contact: Carol Godfrey, 770-832-4403
Southwire Company
One Southwire Drive
Carrollton, Georgia 30119


 
 

/images/buttons/ColumbusOperations_button.jpgColumbus Sees 2.5 Years of Successful OperationColumbusOperation.htm
Register Now Forgot Password?

Columbus Sees 2.5 Years of Successful Operation

Superconductive Power Distribution Comes of Age: Two and a Half Years of Successful Commercial Operation

On February 6, 2009, Southwire Company and its partners marked the two-and-a-half year anniversary of an urban power distribution project using high-temperature superconductor-known as HTS Triax® Superconducting Cable systems.

The installation in Groveport, OH used approximately 200 meters (600 feet) of Southwire's HTS Triax Superconducting Cable to distribute electric power to 8,600 homes and businesses through American Electric Power's Bixby substation. In addition to American Electric Power (AEP), project partners included American Superconductor, the U.S. Department of Energy's Oak Ridge National Laboratory, and Praxair.

"Using second-generation cable design and recent advances in cooling technology, the Bixby installation proves the reliability of HTS Triax Superconducting Cable systems in reducing the cost of high-efficiency power distribution in an urban setting," says David Lindsay, Southwire Director of Engineering, Distribution Applications.

HTS Triax system works worry free

The system has experienced more than 75 transient events, including lightning strikes, during its 2.5 years of operation. Most of these events were through-faults -fault current that entered the Bixby station from the distribution circuits powered by the HTS Triax cable. No change in system temperature or pressure was recorded as a result of the events and the system has never been taken out of service as a result of these events.

The system has operated successfully since its installation in August 2006. Designed and built for a load rating of 3,000 Amps per phase, it performed at 90.5% of the design rating, reaching 2,715 Amps during peak loading in the summer months.

"Our partnership with Southwire has allowed us to test advances in superconductivity and cooling design on our system with virtually no interruption to customers," says Michael Heyeck, AEP Senior Vice President of Transmission.

The many benefits of HTS Triax Superconducting Cable

With the rapid decline in available underground space for conventional cables and the prohibitive cost of real estate for new or expanded substations, superconducting cables are emerging as a solution for electric power to densely populated areas. There are many benefits of HTS Triax superconducting cables, including: · Increased reliability in the electrical grid by facilitating interconnectivity between electrical substations and alleviates substation space constraints. These virtual substations can eliminate the need for some transformers saving a utility customer up to $2 Million per transformer. · HTS Triax cables add capacity to existing duct banks. One HTS Triax cable can carry as much current as 18 large copper cables. This is possible because HTS Triax cable operates at extremely low temperatures for power cable-281°F (-196°C)-and eliminates current flow resistance. · Large power transformers can be located further away from urban centers because HTS Triax cables carry very high currents at lower distribution voltages. Additionally, valuable real estate for development and green space is freed up. · Reduced critical cooling requirements, combined with newly commercialized cryogenic cooling technology, reduces cost and maintenance. HTS Triax is very compact, with three phase conductors placed concentrically around a common central core, cutting the quantity of wire in half. This smaller surface decreases cooling requirements.

More Superconducting Cable installations are at work to support demand

According to Heyeck, "The performance of the HTS Triax system has shown the potential for cost savings with excellent reliability in a variety of applications."

With the Bixby performance success, Southwire now draws on over a decade of in field superconducting experience. Together with projects under way in New Orleans and New York City, these installations prove the in field success of urban delivery of critical electric power through superconductivity and position Southwire as an experienced leader in this innovative offering.

For more information on HTS Triax superconducting cable systems or the Bixby substation project, visit http://www.supercables.com.

Imagery is available to the press by contacting Kayla Smith at kayla_smith@southwire.com

About Southwire:
A technology leader, Southwire® Company is a major wire and cable provider in North America, manufacturing copper and aluminum building wire and cable, metal-clad (MC) cable, metallic and non-metallic flexible conduit, cord products, utility cable products, industrial power cable, power generation cables, copper and aluminum rod and continuous casting technology. Through innovative research, Southwire has developed and patented Flatwire Ready® SureSeal® HTS Triax® Superconducting Cable, SIMpull THHN® cable, Romex® SIMpull® cable and, MCAP® and HCF MCAP® cables. Southwire has also developed other innovative products such as Riser MC cable, HS285, Vibration Resistant (VR2) and PowerGlide® Utility Cables. Visit our website at www.southwire.com.

Press Contact: Carol Godfrey, 770-832-4403
Southwire Company
One Southwire Drive
Carrollton, Georgia 30119