Next Generation in Health Care Cable: HCF MCAP®
Patient care areas of health care facilities are surrounded by metal, liquids and various electronic equipment. As such, the environment yields big potential for stray currents that can be detrimental to patients. Because of these issues, in all patient care areas of healthcare facilities, there is a requirement to provide redundant forms of grounding. To accomplish this, Section 517.13 of the National Electric Code® (NEC®) requires that any branch circuit wiring that feeds patient care areas must have two things: (1) the metal conduit or metal sheath of a cable must qualify as a grounding conductor, and (2) a green insulated grounding conductor must be installed and connected. Traditionally, designers and installers of health care facilities had two choices when selecting their branch circuit wiring: pipe and wire or Health Care Facility (HCF) Type AC cable.
Pipe and Wire Branch Circuits
Pipe and wire is an option that is used for branch circuit wiring in health care facilities. This wiring method requires more planning, has more components, and more installation processes than HCF cable. The pipe is available in a variety of diameters and comes in 10-foot lengths. The pipe is rigid and must be bent in the field as needed to achieve the desired routing. Couplings are required to join the10-foot sections. Once the conduit is installed, the electrician must come back and manually pull the wire through. It’s a lengthy and tedious process. Per section 517.13 of the NEC, the metal conduit qualifies as a grounding conductor and the addition of a green ground provides the redundant ground requirement. While the conduit ground path can be very good, the connection or ground path integrity is only as reliable as the couplings that connect the conduit.
HCF AC Cable
The HCF AC cable option is commonly selected for its advantages over pipe and wire branch circuits. HCF AC cable has wires preinstalled, which means there is no need to pull the wire. It is flexible and continuous which eliminates the need for field bending and couplings. With HCF AC cable, the multistage process of pipe and wire is gone, resulting in both speed and cost advantages. Per Section 517.13 of the NEC, the armor qualifies as a grounding conductor and the addition of a green ground provides the redundant ground. The armor ground path is very reliable because it does not have couplings that can loosen over time, however the ground path performance is not as good as a grounding conductor.
Now there is a new form of healthcare cable that is a HCF Type MC cable product, HCF MCAP® cable, which offers improvements in installation productivity, cost and safety.