|
Designed to excite the senses, Wynn Las Vegas is the epitome of luxury. From around-the-clock gaming to 5-Star dining, every aspect of the resort, officially opened in April 2005, offers guests an exciting chance to beat the odds. The massive landscape - featuring a 48-story hotel tower with 2,611 luxurious guest suites; a 120,000 sq. ft. casino; 15 restaurants; a 1,366 space parking garage; an on-site 18 hole-golf course; approximately 223,000 square feet of meeting space; and approximately 70,000 square feet of retail space - challenged conventional pipe-and-wire installation methods. Thus, to effectively accommodate the unprecedented size and the diversity of the individual installs, architects specified custom-armored feeder MC cable as their ace in the hole. Service and support. The flexibility of Southwire® feeder MC cable made it the perfect solution for Wynn Casino. Unlike conduit, feeder MC is flexible and can be bent to accompany any angle or incline. It’s also easier to install, requiring fewer tools, fewer workers and significantly less time. The variety of the installs changed the game entirely. Accordingly, Southwire supplied custom products to accommodate the unique fire alarm applications for each venue. Additionally, Southwire provided contractor-specified armored communications cable to facilitate continuous communication between venues. |
Advantage goes to the house. When paired with the tremendous time savings MC cable provides over conventional pipe-and-wire installation, the contractor was able to cut overall installation times by 50%. Southwire’s reputation as a one-stop-shop for building wire and cable played a pivotal role in the time savings associated with this project. As a result, the contractor did not have to source out to multiple manufacturers for wire and cable. With Southwire, they had everything they needed. For the project, the contractor was able to coordinate with Southwire’s Starkville service center to create and supply all necessary aluminum and copper feeder MC cable and electrical wiring on an as-needed basis. This provided both Wynn Las Vegas and the contractor with a tremendous time and cost savings. To learn more…
|
![]() |