|
New Busch Stadium is all about the details - just like the game itself. Boasting numerous major-league amenities, including luxury clubs and meeting areas such as Casino Queen Party Porch, Coca-Cola Scoreboard Patio and the Ford Plaza, as well as a Family Pavilion with free batting cages and pitching achines, the Stadium brings fans closer to the game than ever before. And secures Busch Stadium’s place among the top echelon of MLB ballparks. The open-air Stadium consists of three main seating decks with 16,586 fi eld level seats, 3,682 bleachers, and 2,886 standing |
Since the stadium install called for much of the 150,000 lbs of cable to be encased in the concrete foundation, Southwire designed custom 10/8 and 10/12 cable to facilitate the job. This saved a considerable amount of time, since builders did not have to construct the typical supporting structures necessary for pipe-and-wire. One for the record books Southwire’s reputation as a one-stop-shop for building wire and cable layed a pivotal role in the time savings associated with this project. For the project, the contractor coordinated with Southwire’s local service center to create and supply all necessary copper feeder MC cable and electrical wiring on an as-needed basis. The rising costs of copper was of tremendous concern. Since feeder MC cable reduces the number of workers necessary to do the job and requires less equipment to install, the contractor was able to recover their losses in no time, and consequently supplement the cost of copper. When paired with the tremendous time savings feeder MC cable provides over conventional pipe-and-wire, the contractor was able to cut overall installation times by 50%. A fact that made this project a real home run for both the Cardinals and the contractor. To learn more… For more information about Southwire’s complete selection of feeder and branch circuit MC cable, contact us at 1-800-237-4585 or visit http://www.southwire.com/ |
![]() |